AXIS#.MT.TRANSITION

Description

This keyword sets the motion task control word with the motion task transition information.

It takes the following values:

0 No Dwell
1 Dwell
2 Blend into acceleration (after MT end)
3 Blend into velocity (before MT end)

  • Transition Types 2 and 3 (Blending) may only be performed when both starting and following motion tasks are in the same direction. This motion type will turn two motion tasks into a continuous move that only comes to rest after the second move.

  • If Transition Type 2 or 3 is used on motion tasks which alternate direction, the motion tasks will still be performed but will be treated as a Dwell move with zero transition time in between motion tasks.

Examples

Usage

This keyword is used to set what you would otherwise have set with AXIS#.MT.CNTL.

Code

MT.TRANSITION 0 1  Will configure Motion Task 0 to dwell.

Context

See AXIS#.MT.CNTL for more information on the argument semantics.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read Only Array
Units N/A
Range 0 to 3
Default Value 0
Data Type Integer
See Also  

Stored in Non-Volatile Memory

No

Variants Supported

Supported on all drives.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.MT.TRANSITION 0

50e0h

01h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TRANSITION 1

50e0h

02h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TRANSITION 2

50e0h

03h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TRANSITION 3

50e0h

04h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TRANSITION 4

50e0h

05h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TRANSITION 5

50e0h

06h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TRANSITION 6

50e0h

07h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TRANSITION 7

50e0h

08h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TRANSITION 8

50e0h

09h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TRANSITION 9

50e0h

0ah

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TRANSITION 10

50e0h

0bh

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TRANSITION 11

50e0h

0ch

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TRANSITION 12

50e0h

0dh

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TRANSITION 13

50e0h

0eh

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TRANSITION 14

50e0h

0fh

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TRANSITION 15

50e0h

10h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TRANSITION 16

50e0h

11h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TRANSITION 17

50e0h

12h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TRANSITION 18

50e0h

13h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TRANSITION 19

50e0h

14h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TRANSITION 20

50e0h

15h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TRANSITION 21

50e0h

16h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TRANSITION 22

50e0h

17h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TRANSITION 23

50e0h

18h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TRANSITION 24

50e0h

19h

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TRANSITION 25

50e0h

1ah

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TRANSITION 26

50e0h

1bh

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TRANSITION 27

50e0h

1ch

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TRANSITION 28

50e0h

1dh

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TRANSITION 29

50e0h

1eh

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TRANSITION 30

50e0h

1fh

Unsigned8

-

-

Read/Write

No

AXIS1.MT.TRANSITION 31

50e0h

20h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6317

1

6317 (0x18ad)

AXIS1.MT.TRANSITION

Unsigned8[32]

Read/Write

Yes

71853

2

6317 (0x18ad)

AXIS2.MT.TRANSITION

Unsigned8[32]

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.MT.TRANSITION

6317

Unsigned8[32]

Read/Write

-